Part Number: BOOSTXL-DRV8323RS
Other Parts Discussed in Thread: DRV8323, DRV8305, DRV8320, C2000WARE
Tool/software: Code Composer Studio
Hello,
In my design, I use a Picolo F28027F in conjunction with the DRV8323RS, and I use InstaSPIN software. As a user interface, I have the GUI InstaSPIN_UNIVERSAL, which works quite well together.
Now it comes, the GUI does not support the DRV8323 what I would like to customize. Can I use the current GUI (InstaSPIN_UNIVERSAL) as a basis and import it into the GUI composer V2 or is there another way to start? I would like to keep the current setting options and layout of InstaSPIN_UNIVERSAL. Can I add the DRV8323 as a registration page to the current InstaSPIN_UNIVERSAL, much like the DRV8305 SPI does? Or do I have to start from scratch, if so, are there any tutorials that you would recommend? The latest version of the GUI composer is only a cloud version isn't it?
In case I want to modify the current GUI do I have stick on the version 1? How can I use this GUI version, do I need to install CCS 5.5 therefore?
Best regads
Thomas