I cant able to connect my encoder output pin of an induction motor to eQEP block in Simulink. the encoder resolution is 48 pulses per one revolution. while the encoder is connected to the oscilloscope it is showing pulses of frequency 1.5kHz. I cant able to analyze the connection of encoder with DSP f28335