Part Number: DRV8842
Hello,
I am using the DRV8842 to control a brushed12 V DC motor. The MCU I am using that will contorl the DRV8842 is supplied with 5VDC. I am intending to direclty connect the MCU pins (V_Hi = 5V) to the DRV8842 digital pins.
If I understood correctly from the datasheet, only the Vref pin of the DRV8842 is a 3.3 V input, the rest of inputs can be driven with 5V level, is that correct?
Page of the datasheet states that V_iH is 2.2V min and 5.25V max (in the absolute max rating, the max voltage is 7V). What does 5.25V value indicates?
Thank you!