Hi Adam,
The motor I am using has the following characteristics:
- 4 Poles
- 10,000 RPM Max
- 24 volts
I am feeding the controller with PWM set for:
- 332 Hz
- 50% Duty
This should give me 9960 RPM according to the equation:
Fclkin = (RPM/60) * (4 Poles/2)
With Fclkin = 332 Hz
RPM = 9960.
It seems that no matter what settings I try, I can only get the speed up to ~8,000 RPM.
Is this the limit for a 4 pole motor?
Thanks Adam,
Reif Heck