This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8313: Understanding RMS/Peak current and Current limit

Part Number: DRV8313


The datasheet says 'High Current-Drive Capability: 2.5-A Peak'. However, I'm unable to find much more about the output capabilities.

  • The simplified schematic on the cover page shows 3.5A, which I assume must be an error
  • Table 6.1 - absolute max ratings shows Peak output current (OUTx) as "Internally Limited"
  1. What is the current limit. Is it 2.5A?
  2. How is this limit being defined? Is it RMS or absolute peak?
  3. Does the trip current calculation relate to the "internally limited" current limit?

Thanks,
Nick