How does the DRV8813 respond to an open load condition, e.g. one or both phase outputs get disconnected from the target motor?
Does the nFAULT output activate?
Then, how does the DRV8813 respond / behave if the motor is reconnected? Can it "self-recover" and continue running the motor based on the input controls, or does it need its nRESET pin toggled, or ??
thanks