This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8308: Separating VM and Motor power

Part Number: DRV8308
Other Parts Discussed in Thread: DRV832X

Hello support team

Since motor voltage is less than 8.5V, we want to separate VM of DRv8308 and power supply for FET. Motor voltage is 5V.
If VM and motor power are separated, OCP will be happen because motor power is smaller than VM.
How can we prevent OCP? Can we disable OCP by using register OCPTH?

Best Regards,
Hirokazu Takahashi