Hello TI,
Our customer want to design of 48V DC BLDC, Please suggest relevant solution.
Specification as below
Type of Fan : External Rotor
Operating voltage range : 45V- 54V DC
Power Input : 30W
Max. Speed : 300-320 RPM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kundan,
Thanks for posting on the Motor Drives Forum.
A few more questions so that we can suggest a part:
Regards,
-Adam
Hi Adam,
below are the answer
please find attachment for BLDC Spec.