Other Parts Discussed in Thread: LM5109B
Hi,
AM2861 is 33V(max), 3A(output current max) H-Bridge driver IC.
Could you please suggest right TI replace solution .
Warm Regards,
Lin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lin,
TI does not make a direct equivalent to the AM2861 which has the power MOSFETs for the motor drive. The LM5109B is a gate drive solution that is used for motor drive in many applications, the CSD18541 N channel MOSFET is a MOSFET solution that is very small and should be similar to the AM2861 internal FET's.
Confirm if this addresses your questions, or you can post additional questions on this thread.
Regards,