The software path I used: D:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensored
Hardware:DRV8312EVM RevD
I bought a motor control evaluation kit for spinning three-phase brushless (BLDC): DRV8312-C2-KIT,I use the brushless motor matched with the official network and matching procedures.
The motor can run smoothly under the condition of faster speed, large torque and strong anti-interference ability. However, under the control of low speed (50rpm), the motor torque is small and unstable. If the external force is applied to it by hand, the speed will suddenly drop, the anti-interference ability will be poor, and the torque (current) response will be slow.
In addition to the speed of the loop PID, I would like to ask god to know what may be the reason, thank you!