This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: The speed doesn't follow the Pin13 Speed pin acurately in some values

Part Number: DRV10983


Dear People,

We are controlling DRV10985 either by the analog input pin or I2C programing and we found a non continuity point (Abnormal points) at some control values, producing an inestable working point in our servo system.

In our case between 890Hz and 950Hz there is a control gap, no intermediate values can be regulated.

Is there any solution to obtain a continuos regulation?

Thanks in advance.

James Palou