Part Number: DRV8832-Q1
Other Parts Discussed in Thread: DRV8838, DRV8837
Hi,
I am working with the DRV8832-Q1 H-Bridge IC. In the datasheet, there is no information regarding the delay time (between the input and the output signals). There is only information about the 12ms time that it can take from sleep mode to 100% Duty cycle mode (7.3.2).
In my application, I am using two 90 kHz PWM signals (complementary) from a microcontroller, which provides the two inputs of the H-Bridge. But the output is always having an unequal delay time, with a jitter of more than 200 ns. Is this already too high for the H-Bridge? If so, what is the high frequency that is mentioned in the datasheet (7.3.2)?
Thank you.
Regards,
Naveen.