This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Utrasonic generator

Dear Sir,l

I want to design an ultrasonic generator to drive an ultrasonic cleaning transducer. Its Characteristics are as follows:

Type BJC-2850T- 45SS PZT-4
Frequency 28KHz ±1KHz
Power 50w
Capacity 4100pf (pzt4)
Radiating surface 45mm
Resonance Resistance 10-20Ω
Piezoceramics size 35*15*5
Length 82mm
Power Supply Input: 100V~130V or 220V~240V AC
Weight 450g/pcs

Ca you please suggest me the design.

Warm Regards,

Manoj Hiwarkar

9916707384 / 8087764569