I am using the current sense of the DRV8323S Three Phase Gate Driver (8.3.4 Low-Side Current Sense Amplifiers (DRV8323 and DRV8323R Only).
The problem I am having is getting a “correct” current sense output from the DRV8323S driver. The % error ranges from about 14% at 0.5A to about 2% at 4 amps. As the current increases the % error decreases. I am looking for 5% error or better, throughout the range of motor current (0A-10A).
Questions:
- Why is the error range so wide?
- Is the circuit layout correct?
Here are the following details of the test bed:
Schematic: See below
Motor load of 0A - 10A
Current Sense Amplifier Control Register configuration:
Calibration: 0x21C
Normal mode: 0x200
Configured in Bi-directional mode
Gain of 10-V/V
RSENSE = O.025 +- 1%
R182, R183 and R193 are not populated.
Measuring output at TP13
DC motor current is measured using a 3-1/2 digit Fluke
AC motor current is calculated by capturing SOB, using a 6-1/2 digit Fluke, and then calculating the current using the bi-directional equation for current
Looking at the spreadsheet (see below), although the Calculated values are not accurate, there is a considerable difference in % error from 0.5A load to 3.7A load
Any insights would be greatly appreciated.