Other Parts Discussed in Thread: DRV11873EVM,
I am evaluating TI motor drive ICs for a low power cooling fan application, we do not have the motors yet so I am experimenting with motors from consumer drones with the motors free-running (no load).
First motor GARTT Z2205S, 14 poles, 3.5mV/Hz and 32mΩ measured. Similar size to intended application but much higher current rating (and more poles).
Second motor BetaFPV 11000kV (for very small drone), 12 poles, 1.2mV/Hz and 0.12Ω measured. - electrically this is closest to intended application.
First attempts: DRV11873evm with Schottky diodes fitted and a range of resistance values (to form the common connection) – neither motor turns, some jerking on start-up but times out and stops.
DRV10975evm configured over i2c with motor resistance and k
Motor 1 – doesn’t start unless k is increased to about 15mV/Hz then, once running, reduced to 4mV/Hz as the current increases towards current limit. Will not transition to closed loop operation (stalls).
Motor 2 – starts most of the time, but often times out and tries again, usually starts by second attempt. Transitions to closed loop control and can get up to about 8500 rpm (should do 10k).
My experience so far does not fill me with confidence, so – is there a subset of motors that these chips can drive successfully and if so, what specification should I be aiming for in the motor?
We have some flexibility to alter the motor properties at this stage. We want to run a small cooling fan at up to 10000 rpm.
Thanks