This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8825: Heating up of the driver when motor is not connected

Part Number: DRV8825

Hi

I have designed a 2 axis stepper motor driver board using DRV8825 Modules. So the issue that I am facing is that one of the motor is heating up as soon as the power(12V) suppy is connected and it keeps drawing around 1A of constant current. The motor also doesnt work while the other driver on the same board is working absolutely fine and doesnt heat up.