Hi everybody,
I've made a schematic driver control motor use DRV8402/32 but i have problem.With motor DC small my schematic run OK, but normal and large motor not OK. DRV die half bridge.current maximum of startup my motor is 10A, I think my schematic not true. And my schematic have problem : First : I use PWM A control OUT A,B;PWMB control OUT C,D .But I use one PWMA ,PWMB not use(not connect) but still motor run???I don't understand! help me!
The PVDD&VDD isolation GVDD ????
file my schematic :2117.H BRIDGE DRV8432ngly.pdf
thanks