Other Parts Discussed in Thread: DRV8825,
Hi Team,
My Customer wanted to know how to calculate the input and output power of DRV8825? Any input is very much appreciated.
Regards,
Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Renan,
A stepper motor mechanical output power is torque multiplied by speed. The total stepper motor system efficiency is usually mechanical output power (w*T) divided by electrical input power (U/I). Also, the torque is provides by the stepper motor driver should be higher than the system needs to make sure no step pulse missing.
When you talked about DRV8825 efficiency, you may only want to know the power dissipation of DRV8825. In this case, “Calculating Motor Driver Power Dissipation” application note( http://www.ti.com/lit/an/slva504/slva504.pdf ) gives an example.
DRV8825 driver is a current source and provides different step current according to the micro-step setting and full scale current setting. Since the output current and voltage both are changed on every micro-step, I would make s simple case to help on power dissipation estimation or measurement. First, hold the motor not move. If the micro-step setting sets a sine waveform to the motor winding, we can use scope to get the RMS value of that sine waveform. Since the motor is stall, there is no back EMF, use Irms*Irms*Rwinding to estimate the output power. And then, compare it with the input power to get the power dissipation measurement.
Hi Wang Li,
Thank you for your inputs this is much appreciated, the post is for DRV8825. I overlooked that DRV8850 is also tagged and it is my mistake.
Regards,
-Renan