This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8340-Q1: Independent Half-Bridge PWM Mode versus 3x PWM Mode

Part Number: DRV8340-Q1

Hi,

Is there a difference between "Independent Half-Bridge PWM Mode" versus "3x PWM Mode"?

The truth table is the same.  I want to use use this DRV for brushed motor drive.  It has good source/sink capability.

-Kelvin

  • Kelvin,

    Thanks for posting on the MD forum!

    3x mode has the VGS and VDS monitoring enabled which will prevent shoot through within the same phase.

    Independent mode disables this protection so that the 3 high and 3 low gate outputs can be used independently. If you plan on using one phase to drive high and another phase to drive low then 3x mode is suitable for you.

    Regards,

    -Adam

  • Adam,

    Were you referring to "independent MOSFET mode"?  

    I was asking about the "independent half-bridge mode", which does have those protection features as far as I can tell (correct me if i'm wrong).  In section 8.3.4.4 of the datasheet, it explains the differences b/w the various modes and fault responses.

    -Kelvin

  • Kelvin,

    Yes my mistake, I forget that this device has one more mode that the other devices don't have, that's the independent half bridge mode.

    3x PWM mode and independent half bridge mode are very similar but 3x PWM handles the dead time for you (since you don't control the LS FET) while independent you can control it on your own.

    Regards,

    -Adam