Other Parts Discussed in Thread: DRV8873, MSP430G2553
Dear Sir or Madame,
I have an Evalboard with the modulse DRV8873. One Module should drive two Peltier Chips with 4 A and 24V of a TEC.
The Polarity reversal works very well if we put an coil in the circuit.
To reduce the size of the coil we wanted to increase the switching frequency up to 100 KHz.
The DRV8873 ist driven by SPI with the MCU MSP430G2553.
The biggest problem now is that unfortunatly i can't find any further informations, with which frequency the module is currently being driven. And i can not find and informations where i can switch de Frequency.
The GUI for the EVM is already installed. Are there any special registers where i can change the switching frequency? Where can i find this information?
or can we only use the PH / IN2 and EN / IN1 interfaces to inject the switching frequency of 100 kHz?
Thanks for your effort
Yours sincerely
Katrin Ippisch