Other Parts Discussed in Thread: DRV10983, DRV8304, DRV10987,
Hello,
I purchased DRV10970EVM to test my 3-phase sensored DC motor and it worked for couple of seconds and then the on-board fuse popped up and it stopped working. There was no load on the motor and I think the internal voltage regulator which produces VINT for Hall sensors was damaged. I was using three 1.5 kohm resistors to create VINT/2 for negative hall sensor inputs (my motor uses Hall IC) and the sensors need pull-up resistor so I also used three 1.5 kohm resistors to pull them up, so by knowing the fact that the internal voltage regulator cannot provide more than 20mA (based on the datasheet), I guess I damaged it.
The board was purchased for test purpose only, however I know I know I need a higher current motor controller to use in my design. I'm running my motor at 12V input supply to generate 22 oz-in of torque. The below graph shows it would draw more than 2.4A @ 36V to generate 22 oz-in of torque. I searched the TI motor controller directory and couldn't find a motor driver that can provide that much current. Does TI offer a controller that meets this requirement? If not, I'd assume I need to use a pre-driver and power MOSFETs to meet the requirements.
Thanks,