This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2667EVM-CT: DRV2667EVM: How to configure a customized waveform and start the pattern repeatly on Haptive Control Console?

Part Number: DRV2667EVM-CT
Other Parts Discussed in Thread: DRV2667

Hi team,

As title, we are able to configure a customized waveform and add into a specific sequence.

But how are we going to make this waveform to start repeatly ? And how to generate the waveform Hex file.

  • Hi, Oliver,

    Have you tried with the Waveform Synthesizer of the RAM manager? This option allows to create a waveform and repeat it the times that you require. Please go to the RAM manager option in the tools menu of the Haptics Control Console. Select DRV2667 and click on the Advanced button. It will open the Waveform Synthesizer options to mange and create the waveforms.

    Please let me know if you have additional questions or comments.

    Best regards,
    Luis Fernando Rodríguez S.

  • Hi Luis,

    I asked customer to generate the waveform from the advanced option. Also we put them into the sequencer, but when we click start in the GUI, It seems only activate once, can't generate repeatedly. 

    Thanks,

    Oliver

  • Hi, Oliver,

    Do you have a capture of the advanced configuration window with the settings that the customer is using? This would be very helpful for us in order to have a better approach to this issue.

    Best regards,
    Luis Fernando Rodríguez S.