On the DRV8823 datasheet there's a 3.75us blanking time. From what I'm reading this means that the on board comparator ignores current readings for 3.75us.
What is the behavior of the DRV8823 mosfets during this time? The serial interface can operate at 16bits x 16mhz=1mhz so should be able to commanded to turn on/off in 1us which is faster than the blanking time. Does the DRV8823 ignore all commands during the blanking time or is it only the on board comparator is ignored?
We want to implement our own programmable blanking by using a comparator and switch the mosfets off at our own leisure. Is this possible?
What's the maximum speed the DRV8823 h-bridge can be switched from on to fast or slow decay? Thanks!