Hello support,
we have a problem with our motor control hardware, in special with the DRV8302 chip.
In some cases, for about 5% of the parts, we get, sometimes within some weeks, sometimes with hardware older than 2 years the following error:
- nFAULT gets active
- Chip gets hot (more than 50°C)
- Buck converter still works
- VGVDD is ~0V
- shure, the PWM output is dead
- error is NOT recoverable. I assume, that a complete power off / power on should recover the error state !?!
I dont want to publish the schematics here but able to send it per email.
Thanks a lot
Rüdiger