Hi Team,
I got question from customer.
Q.1) When device detects Over current event, how long will it take for output of device being set HiZ?
After Over current fault event, device will start Load Diagnostics.
Q.2) If the fault is still detected during full load diagnostics, which state device will stay?
Q.3) If over current is not detected during Load Diagnostics, will device be in stand_by mode with FAULT pin and FAULT flag are kept asserted?
Best regards,
Nobuo