This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323R: Where is the return path for low side gate drive current? GND or current sense input (SPA, SPB, SPC)

Part Number: DRV8323R
Other Parts Discussed in Thread: DRV8323

The high side driver seems to have a pin specifically for return current, but it is not entirely clear how the return current path is on the low side? And on the variants with no current sense amplifiers, are the SLA, SLB and SLC pins then connected to pull down transistor on low side gate driver? Or is ground used for return current? 

Thanks!