Part Number: DRV8860
Dear,
I am working on the Test Interface that will be used for functional testing of the specific control board at the end of the line and for troubleshooting in the exploitation. I need to integrate 8 channels of general open-drain outputs in my system. Since the DUT (Device Under Test) can be broken it is required that outputs are protected so Test Interface won't fail when the DUT produces short circuit or similar fault. I found DRV8860as very useful for my application and would like to integrate it into the system.
The only concern I have is whether DRV8860 outputs can be referenced to the voltage rail that is different than VM rail? I am wondering whether this can produce open load fault os something similar?
Looking forward to getting feedback from your side.
Best regards.