Other Parts Discussed in Thread: DRV8302, DRV8301, DRV8303
Hi, Team
could you tell me what product would be suitable based on below customer requirement ?
・motor type :BLDC
・Full bridge
・Vbus 15V
・2~3A drive strength
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Masaharu,
We do not have any devices that offer a gate current up to 2-3A. I suggest that you look at the DRV8301, DRV8302 and the DRV8303 because these devices have our highest gate current of 1.7A.
Regards,
Michael