Dear team,
Customer met an issue that when DRV8846 was initially powered on, configuration programed, the motor works normal. Then if they cut off the power then power on again, the motor did not rotate any more.
They asked:
1. If the power sequence of nsleep and enable affect the motor activate?
2. If the decay mode setting affect the start of motor?
3. Will the A1OUT and A2out connection direction to motor have effect?
4. How was the relationship of STEP frequency with A1A2 frequency?
Customer set 100KHz, current 700mA.
Thanks.
Best regards,
Sammi