Hello,
If a system requires DRV8873S-Q1's self-diagnosis of its DISABLE pin function, how can it be implemented? Any ideas?
The DISABLE pin sets the DRV8873S-Q1 output to either an active mode or Hi-Z, so it might need measurement of its output impedance. However, usually a motor is connected, so the result will depend on the motor, too.
Does the DRV8873S-Q1 have a function to achieve it?
Best regards,
Shinichi Yokota