Other Parts Discussed in Thread: DRV2667
Hi TI-team
My customer uses an external MCU.
Jumper MSP has selected USB to provide 3.3V power for TXS0102DCT.
Each signal (SDA, SCL, GND) is connected to the jumper from the external MCU.
It seems that a control signal is being output from the MSP430 to the DRV2667 when the power is turned on.
How do I stop this control signal ?
Do I need to rewrite the firmware or remove the MSP430 or another way ?
Best Regards,
Koji Hayashi