Firstly I thank the community especially Mr Rick Duncan for helping me sort the issue out.
The INAx pins can take either 5 or 3.3v inputs right?and PWm should also be appiled on the same pins?right
let me put this in context.....I am giving it a logic 5v Input for full speed(100% duty cycle).....then I adjust PWM to 3.3v for an appropriate output voltage....can be done right?
Now I have migrated to a 3.3v MCU...which gives 3.3v output for logic HIGH....so how do i make sure that the driver doesnt see this as an PWM input and give me a lesser voltage than motor supply.
How can the driver know that the MCU whether the input supplied from the MCU is a LOGIC level or a PWM signal...
I hope i could give you a clear perspective of what my issue is...
Thanking you,
Jash