Would you be able to confirm that it would be safe to apply +10mA to unpowered LMD18200 H-Bridge switches at each of the two PWM inputs (pins 5 and 17 in our packages) with respect to the SGND and PGND terminals (at pins 8, 18, 19, and 20) for some amount of time, or preferably an infinite amount of time? A “Yes” answer, preferably for the infinite-time case, would be very helpful for a test in unrelated circuitry that would cause this condition to occur.
Please let me know if there are other stipulations regarding other inputs/outputs that would affect your determination.
Thank you.
Ed Riess
Edward A. Riess
Common Control Unit (CCU) Lead Engineer
INTEGRATED MISSION SYSTEMS / L3HARRIS TECHNOLOGIES
t +1 513 573 6220 / m + 513 312 3742
L3Harris.com / Edward.Riess@L3Harris.com
7500 Innovation Way / Mason, OH 45040-9699 / USA