This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8874: Fixed Off-Time Current Chopping, brake vs coast

Part Number: DRV8874


Hello,

This question may be more related to general motor drive theory, but I am hoping someone can help me understand more:

In fixed off-time current chopping, the DRV8874 enters a brake/low-side slow decay state. 

What was the reasoning behind the decision to enter brake/low-side slow decay state instead of entering coast/Hi-Z state for current chopping?

Thanks,

Andrew

  • Hi Andrew,

    In fast decay, the current decays towards zero as fast as possible. This method is also called Coast since the motor coasts to a stop. This behavior is due to the motor speed being proportional to the voltage across the motor. During fast decay, the current will decay quickly because a voltage of greater magnitude but the opposing polarity is applied to the inductive load when driven.

    During slow decay, the current decays slower than fast decay. The motor brakes instead of coasts to a stop. This mode is referred to as Brake. Slow decay occurs by disabling the Forward direction’s high side FET and enabling the Reverse direction’s low side FET. Slow decay is also called active freewheeling.

    As for your question, the reason why the device uses slow decay/brake is that more torque can be applied to the load as the current decay rate is slower.

  • Excellent, thank you Hector.