This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8850: Is VPROPI output proportional to the sum of currents in the

Part Number: DRV8850


Hello,

I'd like to use half-bridges in the DRV8850 in parallel (OUT1 and OUT2 connected together), and connect the motor between this combined output and ground.  I expect that I can drive the motor with more current that way.  I only need to turn the motor in one direction.  Each MOSFET in the bridge has got an individual logic control input.

I need to limit current during motor startup, or accidental stall.  I'm reading 7.3.3 in the datasheet, and my question is about current sensing in DRV8850.  Is the current out of the VPROPI proportional to the sum of current in the high side MOSFETs?

Best regards,
- Nick

p.s.  If the pin VPROPI outputs current proportional to current flowing in the bridge, shouldn't it be called IPROPI?