This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8874: Power Sequence Confirmation

Part Number: DRV8874


Hi team,

Is it allowed to input the control signal before inputting the VM?

Please tell me both EN High and Low case.

The reason why asking this question is that the customer is considering whether this device gets into failure/broken or not.

Thank you for your support.

Best Regards,

Kazuki Kitajima

  • Hi Kitiajima-san,

    Yes, it is allowed to input the control signal before inputting the VM.

    Please see the second paragraph of section 7.3.2 Control Modes.

    The inputs can accept static or pulse-width modulated (PWM) voltage signals for either 100% or PWM drive modes. The device input pins can be powered before VM is applied with no issues. By default, the EN/IN1 and PH/IN2 pins have an internal pulldown resistor to ensure the outputs are Hi-Z if no inputs are present