Hi,
i would like to ask you a question about output linearity, Fig13 and Fig14 (datasheet page 8).
I suppose the input voltage scale of the Figures seems to be incorrect...
For example, in case input is around 1.6V then output is 60V @Vbst=105V/Gain =40.7dB.
I think in case input is 1.6V, output will be 1,6*40,7dB = 173V ---> 86.4V.
Will you tell me what is my misunderstanding?
Thank you for your support.
Best Reards,