This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8870: Using DRV8870 without thermal pad connected

Part Number: DRV8870

I intend to use the DRV8870 for a very low power operation (10mA max), and clearly don't need the thermal pad.  For the simplicity of building a prototype by hand, can I operate the DRV8870 without the thermal pad in this low power mode?  The power dissipation would be 10mA^2 x 0.35 ohms ~ 35uW which wouldn't heat up a standard SOIC-8 package.  I just wanted to insure the design didn't rely upon that pad being grounded.