Other Parts Discussed in Thread: DRV8412, DRV8800, DRV8844
Hi,
I am using the DRV8872 to drive a voice coil (inductive load).
I have made a test with PWM running at frequency of 100kHz and D=50%. The VM was supplied with 12V and ISEN was shorted to GND.
I have observed a jitter in the output signal which caused further problems in my system. The jitter was caused by the non constant propagation delay in between input signal (both rising and falling edge) and output signal and was in between 700ns and 800ns (the whole pulse was jittering).
Is this a normal behaivour of the DRV8872?