This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8703-Q1: Diagnostic information

Part Number: DRV8703-Q1


Hi,

we would like use the DRV8703-Q1 to drive a DC motor. On the datasheet we have seen that there is a FAULT Status register that provides some diagnostic fault: Overcurrent, undervoltage and overtemperature.

For our application we need also the following diagnositc feedback: short-circuit to ground, short circuit to battery and open load detection.

Using a particular type of control driving or a particular configuration, it is possible do these diagnosis?

Thanks.

Andrea

  • Andrea,

    For short-circuit to ground, VDS status register Hx_VDS would report.

    For short circuit to battery,  VDS status register Lx_VDS would report.

    But, DRV8703_Q1 doesn't support open load detection. You may have to build your own circuit to detect it.