Dear TI and experts,
We have designed in DRV8703-Q1 on a board. It seems to operate just fine. Except that the Vso pin (current measurement output pin) goes to 0V when no current is flowing.
According to the datasheet top of page 25 an offset should exist (Vio*Av). This is also depicted in figure 34. That means that when the motor current is 0A, an output of around 0.4V should be present on the Vso pin when the Av is set to 78. But that is not the case. At 0A the Vso pin is still 0V. However as soon as the motor is started the Vso pins generates an amplitude.
To be sure, we have confirmed the same behavior directly on the evaluation board.
We have also again to be even more certain read back the amplification in the config register bit 0 and 1 and confirmed that Av is set to 78. => 5mV*78 ~ 0.4V @ 0A in sense resistor.
Can you please inform us if there is a mistake in the datasheet?
Best, Christian