Hi,
My customer is concerned about the lifetime impact from powering their DRV8340-Q1 from a 48V source based on footnote #2 (page 8 of DS) mentioning 24V systems. I interpret the footnote as below. Can you please confirm if it is correct and if there is a lifetime impact when operating at nominal voltages close to 50V?:
Footnote #2 is just specifying that the electrical characteristics table is valid for up to 60V transients, but the device is intended for use up to 50V continuous. The 5.5V to 50V specification covers the voltage ranges for most applications powered directly from a 12V or 24V automotive battery, but you can also power from a regulated source that will not exceed 50V continuous.
Thanks,
Antonio