This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8313: Comparator COMPN pin low issue

Part Number: DRV8313

We have voltage divider connect to this pin, 10K to GND and 3K to V3P3, and 10K to /COMPO and /RESET. COMPP is connected to a thermistor for over temperature control. We have this circuit working fine for 30 boards, but 3 failed due to COMPN is 0.2V after they working for a while, we cut the trace from the divider to PIN22 (COMPN), then the voltage divider works normally.  Then it must be the problem of the chip, what could be wrong there, can we get help from the factory to investigate that? 

Thanks,

Frank