Other Parts Discussed in Thread: TMS320F28379D, , DRV8332
I am searching DC brushless motor driver.I plan to control this driver with DSP TMS320F28379D.
According to following E2E, it was written TMS320F28379D can perform FOC processing period is 460ns.
To perform this period, I think it will better to choose high PWM frequency motor driver.
For example, gate driver DRV8353's recommended fPWM is MAX 200kHz.
On the other hand, FET included driver DRV8332's recommended Fsw is MAX 500kHz.
I think this frequency is depend on FET's gate resister and gate capacitor.
Please tell me how the fPWM specification of the gate driver is determined.
Is it better to use a driver that includes an FET like the DRV8332 to achieve a high PWM frequency?