Other Parts Discussed in Thread: PCA9306
Help to evaluate drv10975rhfr / vqfn: the system is powered by 12V, and the output power consumption is about 2.2W (several hundred MA); at the peak, the system will have 2.5A current in an instant
Question:
1.1 pin4 I think some reference designs are connected with inductors and some are resistances. Please help to confirm!
1.2. Does pin4 need a diode? If so, what is the role? (I think some references are connected; some are not connected with diodes.)
1.3. If pin4 is to be connected to diode, what are the requirements for selection?
2. How to design pin5? (I see the reference design, some are directly grounded, some are connected to capacitors)
3.1. Is pin9 the internal output voltage of the chip 3.3V? Can this voltage supply the external u41 U60? (u41 U60 is a level conversion chip, which is also ti's)
3.2. When I check the specification, there will be 1.8V and 3.3V voltage output inside the chip? Which pin does the two voltages correspond to?
4. Pin10 pin11 / SCL SDA communicates with I2C on the other side. The voltage is unbalanced. Is u41 OK? (as shown below)
5.1. Pin12 FG is connected to our Bluetooth chip, but the Bluetooth chip is a 1.8V I / O port. Can I / O port of Bluetooth be directly connected to pin12 FG? Or it needs to be designed as shown in the figure below. It needs to add level conversion chip U60 to connect the two side network?
5.2. Does pin12 FG need pull-up resistance?
6.1. Pin13 speed is connected to our Bluetooth chip MTL? PWM network. But Bluetooth chip is a 1.8V I / O port. Can I / O port of Bluetooth be directly connected to pin13 speed? Or it needs to be designed as shown in the figure below. It needs to add level conversion chip U60 to connect the two side network?
6.2. Does pin13 speed need pull-up resistor?
7. What is the function of PIN14 dir? Do you need to pull up or down? If necessary, pull up or pull down? Do you need anything to control it?
8. Is the pin15 pin16 directly connected to the earth when routing, or is it led out to the designated earth separately?
9. Is there any problem with pin17 ~ pin21? Are beads in series required? Shunt capacitor? Wait...
10. Have the capacitance values of pin23 and pin24 for capacitors met the above power operating conditions?
11. Ask pin12 FG again. If the conversion level chip is used, what is the maximum frequency that FG can support? How many frequencies can pca9306 support under corresponding conditions? (we are worried that the signal transmission of FG can not keep up with the demand)