Hello,
I am using the DRV8701 to control an H-bridge. The power supply is a 24V battery and the motor's stall current is about 200A.
I need to include TVS diodes at the motor's terminals to get the product certified. Now, my question is how high should the TVS breakdown voltage be to avoid problems with the DRV8701 and with the FETs.
I was thinking of a 28V breakdown because the full-charged battery will be higher than 24V and I don't want the TVS to conduct at normal operation. However, their clamping voltage goes up to 45V, which should be ok for the DRV8701, but is higher than the Vds of the FETs (40V). Is this going to be a problem because the FETs will breakdown before the TVS? Should I change to 50V or 60V Vds FETs?
Thanks!