Other Parts Discussed in Thread: DRV8711
Tool/software: Code Composer Studio
HI,
I am working on DRV8711 with Delfino79D and brushed DC motor, in TOFF register i set PWMMODE bit to 1 for Direct PWM signals from the MCU, and i ask if i can use internal indexer mode to control the rotational velocity or change the duty cycle applied on the motor, ask also if the internal indexer is used only for stepper motor types or not and what exactly it is used for !