This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8306: When DIR is reflected to Gate Drive signal

Part Number: DRV8306

Hi Team,

I have two questions regarding the timing when DIR is reflected to Gate Drive signal as following. 

1. When changing the direction of rotation, how long does it take from changing the DIR input to being reflected in the gate drive output?

2. Is it ok to change the DIR logic during Twake at start up timing?
According to the datasheet, we need to take care about logic change timing at Twake for IDRIVE and VDS. So I want to double check just in case  if we need to take care DIR as well in the timing.

"The hardware inputs (IDRIVE and VDS) are latched during the wake-up time (tWAKE). Any further change to these pins is ignored unless a power-up cycle or an ENABLE pin transition after sleep mode occurs."

Regards,

Takashi Onawa