This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1: Motor Selection for Headsup Display design

Part Number: DRV8889-Q1

I want to use this motor driver DRV8889-Q1 in my heads-up display project. I need some guidance to choose the right stepper motor which would be compatible with this driver. 

Some factors to consider :

1. Range of Voltage: 4.5V - 45V

2. Continuous Current - upto 1.5A ( looking for a lower current rated motor)

3. Step Angle/Resolution - 0.5 to 1 degree

Any help in making the right selection would be appreciated.  

Some useful links:

Reference Design- http://www.ti.com/solution/head-up-display-hud

Driver- http://www.ti.com/lit/ds/symlink/drv8889-q1.pdf?ts=1588015073753

Article- https://learn.adafruit.com/all-about-stepper-motors/matching-the-driver-to-the-stepper