hello,
I want to run 48V / 2.1A, BLDC motor but I am not able to find driver IC for my suitable range.
source input is: 12 - 36VDC / 10A Solar power or 24V DC Batteries.
Load Output: 48V / 2.1A , BLDC Motor.
I want a Driver IC which Buck/Boost the power at the same time it will charge the batteries.